AXIS#.MOTOR.TBRAKERLS
Description
This parameter is used to configure the mechanical delay when releasing the motor brake. AXIS#.MOTOR.TBRAKERLS is a time delay that is applied when a brake exists and the drive is enabled. When the drive is enabled, the brake is commanded to release and, during the AXIS#.MOTOR.TBRAKERLS period of time, the drive does not accept a motion command. This delay allows the brake to fully release before the drive begins a new motion.
-
-
If AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.2 or greater, this parameter will be automatically configured for Kollmorgen motors.
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
ms |
|
Range |
0 to 1,000 ms |
|
Default Value |
75 ms |
|
Data Type |
Integer |
|
See Also |
N/A |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.MOTOR.TBRAKERLS | 0x500B | 0x1B | UINT | - | - | RW | False |
| AXIS2.MOTOR.TBRAKERLS | 0x510B | 0x1B | UINT | - | - | RW | False |